用TPS53819A做一款微型DC/DC电源,输入4~20V,输出3.3V,最大工作电流有时可能到10A以上,正常情况在5A左右。按PDF文档画的线路板,只是开关管用的是2只英飞凌的管子,焊接好后无输出。发现可能是TPS53819A管子的驱动电压比较低,外接的英飞凌管子没有完全打开。后把开关管去掉测试驱动波形,主开关管波形如附件,可以说是杂乱无章,按理应该是很正的方波才对,求支招,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用TPS53819A做一款微型DC/DC电源,输入4~20V,输出3.3V,最大工作电流有时可能到10A以上,正常情况在5A左右。按PDF文档画的线路板,只是开关管用的是2只英飞凌的管子,焊接好后无输出。发现可能是TPS53819A管子的驱动电压比较低,外接的英飞凌管子没有完全打开。后把开关管去掉测试驱动波形,主开关管波形如附件,可以说是杂乱无章,按理应该是很正的方波才对,求支招,谢谢。
Hi
如果给反馈,芯片能正常输出类似方波,基本上可以认为芯片没有问题。(你的测试存在问题,同时建议测试一下Vreg电压需要在范围内)
有可能是你选择的MOS存在问题。