Hi,
现在用LP8860做屏背光驱动,想要配制EEPROM
要求:输入12Vdc,输出27Vdc,电流4*80mA, 电流控制方式PWM输入控制
1,有没有EEPROM配制参考?
2,首次EEPROM配制好后,每次起机是否都要重新写入?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
现在用LP8860做屏背光驱动,想要配制EEPROM
要求:输入12Vdc,输出27Vdc,电流4*80mA, 电流控制方式PWM输入控制
1,有没有EEPROM配制参考?
2,首次EEPROM配制好后,每次起机是否都要重新写入?
EEPROM用于存储LP8860的控制模式及各种参数,,设计者可根据应用手册 http://www.ti.com/lit/an/snva757b/snva757b.pdf 来选择对应的版本。 LP8860-Q1使能后,首先读取EEPROM值并拷贝到对应的寄存器,软启动开始并升压输出。
2. 根据table1, H版本的VDD是5V且禁止内部的charge pump, 如果VDD是3.3V则需时能charge pump, 则EEPROM 0x70值由C4改为C5, 0X76值由8C改为8E. 如有其他的需求,则更改相应的EEPROM的值即可.
3.MCU/处理器可对EEPROM进行重新烧录,出厂时烧录一次即可, 出厂后升级可重新烧录,但不要超过1000次 。烧录流程如下.
1. VDDIO/EN 脚拉高使能LP8860-Q1
2. 解锁EEPROM,解锁代码写入寄存器0X1A,
a.写0x08到0x1A寄存器
b.写0xBA到0x1A寄存器
c.写0xEF到0x1A寄存器
3. 写入EEPROM,配置值依次写入0x60~0x78寄存器(每写一个寄存器等待20uS)
4. 开启EEPROM 烧写,写0x02到0x19寄存器,
5. 等待200mS
6. 完成EEPROM 烧写,写0x00到0x19寄存器.
注意:在烧录EEPROM前,需禁止PWM和PLL。