This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8860 EEPROM 配制

Other Parts Discussed in Thread: LP8860-Q1

Hi,

现在用LP8860做屏背光驱动,想要配制EEPROM

要求:输入12Vdc,输出27Vdc,电流4*80mA, 电流控制方式PWM输入控制

1,有没有EEPROM配制参考?

2,首次EEPROM配制好后,每次起机是否都要重新写入?

  • EEPROM用于存储LP8860的控制模式及各种参数,,设计者可根据应用手册 http://www.ti.com/lit/an/snva757b/snva757b.pdf 来选择对应的版本LP8860-Q1使能后,首先读取EEPROM值并拷贝到对应的寄存器,软启动开始并升压输出

  • 1根据应用手册SNVA757B中table1, . 当前设计可以使用H版本的芯片,或者使用其他版本芯片并烧录H版本的EEPROM值,H版本的EEPROM值见table18,对应的原理图为figure 8

  • 2. 根据table1, H版本的VDD是5V且禁止内部的charge pump, 如果VDD是3.3V则需时能charge pump, 则EEPROM 0x70值由C4改为C5, 0X76值由8C改为8E. 如有其他的需求,则更改相应的EEPROM的值即可.

    3.MCU/处理器可对EEPROM进行重新烧录,出厂时烧录一次即可, 出厂后升级可重新烧录,但不要超过1000 。烧录流程如下.

    1. VDDIO/EN 脚拉高使能LP8860-Q1

                 2. 解锁EEPROM,解锁代码写入寄存器0X1A

                                         a.0x080x1A寄存器

                                         b.0xBA0x1A寄存器

                                         c.0xEF0x1A寄存器

                 3. 写入EEPROM,配置值依次写入0x600x78寄存器(每写一个寄存器等待20uS

                 4. 开启EEPROM 烧写,写0x020x19寄存器,

                 5. 等待200mS

                 6. 完成EEPROM 烧写,写0x000x19寄存器.

     注意:在烧录EEPROM前,需禁止PWMPLL

  • 4. 烧录校自校验

     在实际的操作中,EEPROM的烧录通常由处理器或MCU完成,这样可以简化生产流程以及方便后续的升级。如果烧录失败,LP8860-Q1则无法正常工作,为此,可靠EEPROM烧录及校验是非常必要的。以下给出了一种EEPROM烧录后的自校验方法,省去了生产线上单独为LP8860-Q1烧录EEPROM的工序,系统升级时,将烧录成功标志位P_S清零后,即可实现对LP8860-Q1 EEPROM升级配置。

  • 您好,请问fpd-link iii你调通了吗?

    希望联系到您,解决该方案(925+940)的问题!

    请加QQ:173490506