This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

帮推荐一个I2C通讯协议的IC,具体要求如内容。

Other Parts Discussed in Thread: BQ40Z50, BQ34Z100-G1

放电过流保护电流   <9A        
保护板过电流   >5A        
过放保护检测电压 (3.0±0.05)*n(V)          
过充保护检测电压 (4.28±0.05)*n(V)          
连接器型号   待定        
NTC电阻   10K±1%        
电量计   需要,请提供IC型号        
电池线径,颜色 B+ 红色2pin,24号线        
  B- 黑色2pin,24号线        
  NTC 黄色10K,24号线        
  I2C_SDA 白色,接口电平3.3V,24号线        
  I2C_SCL 蓝色,接口电平3.3V,24号线        
电池输出可关断输出   带,主机通过I2C发指令给电池,可以关断电池输出,插入适配后可激活