输入电压42V, 准备用16010输出15V /1A。手册上说可以最大输出50V, 可是webench却算不出来。 请问这款芯片能否稳定输出15V,外界电感、电容应该怎么配置。谢谢大家。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
输入电压42V, 准备用16010输出15V /1A。手册上说可以最大输出50V, 可是webench却算不出来。 请问这款芯片能否稳定输出15V,外界电感、电容应该怎么配置。谢谢大家。
您好,16010可以稳定输出15V/1A,电感选取主要考虑到最恶劣工况下电感不能发生饱和,因此取最大输入电压对应的电流纹波最大,电感最可能发生饱和,此时为最恶劣工况条件。具体计算过程可以参考datasheet。其中Kind是最大输出电流的纹波系数。
输出电容主要考虑到输出电压纹波,环路稳定性以及负载突变下电压over/undershoot(峰值电流控制下输出电容和负载会构成一个低频极点)。输出电压纹波主要考虑电容上ESR以及电感电流纹波在电容上的影响。 另外在负载突变的时候电容会受瞬态性能指标的限制,系统需要快速调节电压。可参考datasheet分别对应负载突然加重和负载突然变轻对应的电容最小值。
希望这能帮助到您!谢谢
如果你的负载条件是1A,建议选择输出电流为1.5A的较好,留有一定裕量
你好,
理论上来说是没问题,不见得就没问题,最好实测下thermal 性能,谢谢。