问题:当电路处于充电状态时,打开系统电源开关SW2,充电指示灯开始闪烁,充电故障!保持系统开关打开,重新插拔adapter,充电正常。适配器电压为15V
我把r1用导线短路,这个问题依然存在
我用示波器测量输入电压,在上电时输入电压有波动的现像,开关上电后15ms就稳定了。不清楚是不是跟这个有关系,如果是电压异常,那稳定后应该可正常充电,但这个故障必须断开适配器重新接入才能恢复。
请问是什么原因导致的?如何解决?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我现在把R1采样电阻改成了5毫欧,另外把充电电流设置为1.5A了
按下SW2之前,用万用表测得电池电压为11.16V,充电电流1.5A,适配器电压15.12V,C1两端电压为15.09V,状态灯指示为充电
按下SW2之后,用万用表测得电池电压10.94V,充电电流为0A,适配器电压15.19V,C1两端电压为15.18V ,状态灯闪烁
抱欠,我手上没有电流探头,所以有就直接用示波器测量的r1两端的采样电流
可以看出,由于容性负载的原因,电压波形有两次跌落,第一次跌落幅度约为6V,第二次跌落幅度约为2.5V,两次间隔时间大约为21ms
电流由于是直接测的5毫欧电阻的采样值,信号太弱,所以看不出实际电流,但波形上还是反应出来了,有两次大电流,第一次峰值电流很高约为400mV对应80A的瞬间电流,第二次约为70mV对应14A的瞬间电流。两次间隔时间与电压跌落时间相符合约为21ms。
这个灯闪烁不充电,有没有可能是芯片检测到过流了,所以停止充电?但如果是芯片检测到过流停止充电,附载上电完成后,过流解除应该可以自动进入充电状态才是吧?