This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61021A电感选择

Other Parts Discussed in Thread: TPS61021A

根据典型电路,计算电感峰值电流如下:

VIN=1.8V

IOUT=1.5V

VOUT=3.3V

VIN=2.4V

IOUT=2.5V

VOUT=3.3V

VIN=3V

IOUT=3.5V

VOUT=3.3V

电感峰值电流

3.54A

4.24A

4.56A

请问这种情况下,电感选择XFL4015-471ME(DCR:8.36,SATURATION CURRENT:6.6)是否可行?一般饱和电流比峰值电流大多少合适?