This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

两节18650并联,有没有合适的充放电管理芯片及升压芯片?

Other Parts Discussed in Thread: BQ25895, TPS61088

方案是这样的,充电适配器可以任选,5V2A/3A或9V2A/3A都可以,给两个并联的18650充电,一种 方案是用充放电一体的芯片,可以升压输出,但输出电流要到3.5A-4A之间,总功率20W左右,然后接一个恒流源芯片。另一种方案是用充电管理芯片,输出电压电流直接从电池获取,因为电池电压范围是2.8-4.3左右,所以要用到一款低电压输入,高压高流输出的升压芯片,电流也要到3.5A-4A,总功率也要20W左右,后端再接恒流源芯片。对TI芯片不是很熟悉,请大神给推荐,谢谢了

  • TI有没有锂电池充放电一体的芯片?输出5V的电压,电流最高可以到多少?

    或者输出高于5V的电压,6V 7V 8V 9V 10V等,但总功率在18W左右的,有没有类似芯片?

    如果没有这类芯片,那就只能用充电芯片,电池直接放电,这就需要低压输入,大功率输出的升压芯片,输出功率在18W左右,接恒流源芯片。

  • 单串充电芯片,目前TI的OTG大部分都是只支持5V,可以看一下BQ25895,OTG最高可以支持到3.1A,实际看发热情况能做到多高。

    升压芯片目前常用的是TPS61088,可以用WEBENCH 选型一下,http://www.ti.com/design-tools/overview.html