我使用的贵公司buck降压芯片TPS562219,电路图入上图所示,当R1为3K-23K左右时,芯片可以正常工作,输出大概1V-3V,芯片5脚SS端输出一个高电平。但是我将R1换到33K以上时,芯片就不工作了,芯片5脚SS端输出一个锯齿波。我想要的工作电压是输出5V,所以现在不能用,也没有找到原因是什么,请问贵公司是否知道原因在哪里?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
没有看到电路图,请问你的输入是多少?负载多大?
需要注意这个芯片最大推荐的duty是65%,所以输入电压不能太低(注意留些buffer)。同时必须有足够的稳压电容尽量靠近芯片Vin脚(防止瞬态被拉地)。
负载3欧姆,输入11-15V,Vin端有20uF电容。
我之前不知道这个电路要工作在占空比65%以下,在我的应用中占空比要在75%-100%,所以这个芯片我用不了了。
在我的应用中,buck电路输入电压在5V-10V,输出电压稳在5V,输出电流1A,请问贵公司有没有可以推荐的buck芯片?