This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS562219在输出1V-3V左右时可以正常工作,在输出3.2V以上时不工作,输出电压为0V。

Other Parts Discussed in Thread: TPS62150A, TPS62150

我使用的贵公司buck降压芯片TPS562219,电路图入上图所示,当R1为3K-23K左右时,芯片可以正常工作,输出大概1V-3V,芯片5脚SS端输出一个高电平。但是我将R1换到33K以上时,芯片就不工作了,芯片5脚SS端输出一个锯齿波。我想要的工作电压是输出5V,所以现在不能用,也没有找到原因是什么,请问贵公司是否知道原因在哪里?