Other Parts Discussed in Thread: LM2735, TPS61175, TPS63020, TPS61085, TPS54610
如题,之前用TPS63020,但是焊接成品率好低。要换一个,我看到有LM2735,TPS61175和TPS61085,但是例程和webench没有这几个的设计,是因为这几个芯片无法满足需求,还是因为设计库中没有这几个相关电路?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
建议用专门的升降压芯片来做,相对比较简单: http://www.ti.com.cn/zh-cn/power-management/non-isolated-dc-dc-switching-regulator/buck-boost-inverting/converter-integrated-switch/products.html
如果你用热风枪焊接QFN这类封装,是非常容易的。如果只有烙铁确实焊接比较麻烦。
而现在SOP这类有封装的芯片相对比较少,可以选择一些升压芯片来做,但是相对电路就麻烦很多。
54610的原理图,测试结果,Geber在这个连接下
http://www.ti.com/tool/PMP2440?keyMatch=null&tisearch=tidesigns-power
| PMP2440.1 (Output Voltage 1) | |
|---|---|
| Vin (Min) (V) | 3 |
| Vin (Max) (V) | 5.5 |
| Vout (Nom) (V) | 3.8 |
| Iout (Max) (A) | 1.5 |
| Output Power (W) | 5.7 |
| Isolated/Non-Isolated | Non-Isolated |
| Input Type | DC |