我们在调试LP87524时遇到了一个很奇怪的问题,BUCK0/BUCK1/BUCK2输出比较正常,当BUCK3的负载电流大于800mA时,LP87524所有通道的电压都会随着输出电流的增大而增大,直到2A左右输出就保护了,所有通道输出关闭,但是BUCK3的额定输出电流时3.5A,在BUCK0/BUCK1/BUCK2这几个通道上就不会出现这样的问题,也不会影响其它通道。请问有没有相关的配置参数文件提供给我们参考一下?或者可能哪部分电路会影响到这里?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
电流增加后,其他路电压增加时万用表测试的吗?用示波器测试一下,很可能是不稳定造成示数上的偏高。
确实很可能是布局的问题,Layout上模拟GND和功率GND是要分开,不然是容易造成不稳定。但是在你的Layout,或许还要考虑各组输出之间的Layout,以及整体GND的Layout.