這個是應用於UCC28063與UCC25600於輕載中的PHB相位控制是否輸出的電路應用,而於第四頁中的電路圖上,D11/D12,D1/2, 該如何連接?是全部與A/B二個全部相連接,或是相位PHB,是單獨電路,不與UCC25600 OC PIN3,相連接?請指點迷津,也請TI 工程師弄清楚一點,不然Layout下去又沒有效果,如果產生炸機,那又找誰Debug,再來又要割PCB, 那就非常麻煩,請各位TI工程師確認一下,圖放下去時,請再確認一下,不然使用工程師是要用猜的嗎?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
關於http://www.ti.com.cn/cn/lit/an/snva796/snva796.pdf檔案外加電路上,貴TI 工程師們,是否有實際測試過,實戰過,可以立馬上機測試,沒有問題,還是只有理論值,讓我們拿貴公司的IC來作產品的工程人員,當白老鼠試驗,目前我司使用UCC28063+UCC25600做成輸出58V*8.5A 的LED Driver, 於輸出3A左右還有88%效率,但輸出到2A左右,輸出約100W左右,但輸入是175W 左右,所以目前我UCC28063 PHB PIN4是接在VREF PIN15上,所以應該是二相PHA/PHB都啟動,才會有這個問題,還是LLC變麗器調整不好,才會這樣,請TI工程師們,來解惑一下,謝謝。
這個電路圖連接,是在http://www.ti.com.cn/cn/lit/an/snva796/snva796.pdf檔案的第五頁,Figure 4. External Phase Control Circuit With the UCC28063 and UCC25600,您可以看檔案中的圖中連接,那要問原廠TI 工程師,您們內部需確認,那不是我自已繪製電路圖,是TI內部所發出來文件,敝人是無法看到原版電路圖,還有原始電路版,所以才會上網向貴公司求證,原圖可以去看snva796 檔案第五頁第4圖,原本圖如下:
如果四點全部相接如下:
UCC256200 OC PIN3 是與UCC28063的控制PHB電路是分開如下圖:
是請您幫忙向TI原作者來確認是何種接法,因為我可能無法找到原作者,去確,勞煩您們去確認一下,謝謝。