附件电路是基于LM3150设计的恒流源电路,激励部分是WEBENCH设计的24Vin,5Vout-12A电路,下面电路实现恒流控制。现在的问题是在0-3A范围内可以实现很好的恒流,大于3A电路进入非线性,在4.5A左右既进入饱和,无法实现原设计的12A电流输出,试过更换更小RdsoN的管子,电路无改善。请各位大神指点一下问题所在。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
附件电路是基于LM3150设计的恒流源电路,激励部分是WEBENCH设计的24Vin,5Vout-12A电路,下面电路实现恒流控制。现在的问题是在0-3A范围内可以实现很好的恒流,大于3A电路进入非线性,在4.5A左右既进入饱和,无法实现原设计的12A电流输出,试过更换更小RdsoN的管子,电路无改善。请各位大神指点一下问题所在。
Hi
电感选择饱和电流建议大于16A以上.
MOS Rdson关系到效率,建议选择Qg尽量小的MOS, 牵涉到芯片温升,驱动能力等。
做恒流,特别是你电流比较大,layout会很重要。
你好!谢谢回复! 电流问题基本找到原因了,OPA211电源电压5V时造成后面的驱动能力不够,换成15V电源,电流就上来了,限于手头的负载,目前可调到8A左右。现在有一个新问题,电流大于6A以后LM3150的输出电压随电流增大而增加???电压输出由4.5A时的5.2V一直增加到了7A时的6.47V(WEBENCH设计时参数是5V稳压输出)。 请问一下,这是什么原因造成的呢?LM3150不是应该是恒压输出吗?