Other Parts Discussed in Thread: TPS2561
1、关于TPS2561的应用,用负载仪一直增加OUT1的负载(OUT2空载),直到加载了5V/1.3A负载时触发了过流保护,但这时只是OUT1变成了3.6V/1.3A,OUT2不受影响仍是5V/0A,INPUT变成了5V/1.3A。Fault1仍是高电压(过流后不是应该变为低电平吗?)上述状态持续了10分钟后,测量2561的温度为 65度左右。
问题1:上述的情况正常吗,2561的过流保护模式是怎样的,电流不变电压变低吗?如上述情况,INPUT = 6.5W,OUT1 = 4.68W,大约有1.82W 持续损耗在2561上导致2561发热,由于我们的样机的GND很大散热很快,实际测量起来并不是很热。但是如果2561的过流保护就是这样电流不变、电压降低的话,把限流阀值设置成2A以上岂不是有更大功率消耗在2561上、把2561烧掉都有可能?
问题2:为什么过流后FAULT脚没有变化?