我的TPS25617B及相关供电部分刚刚焊接好,AM3359芯片还没有焊接。
我上电试了一下,SYS和LDO1在上电时分别为5V和1.8V,但是过了5S以后,这两个电压就都没有输出了。
其它DCDC和LDO2/3/4自始至终没有输出。
使用万用表测量过各路LDO/DCDC输出阻抗,均正常,没有出现任何对地短路现象,未监控过SYS的PWM抖动。
按照TPS65217B对AM3359ZCZ供电ACTIVE时序图来看,STROBE 15所显现的SYS和LDO1上电既有输出的现象在我的板子上显现出来了。
而由于AM3359芯片未焊接,因此没有提供WAKEUP#和PWR_EN信号的来源,无法进入ACTIVE状态。
我的疑问是,在此种状态下,经过5秒钟后,SYS和LDO1就会自动断电,此现象是否正常,在相关DATASHEET中未发现对此种工作模式的描述。