This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于chem_ID



刚计算出来的chem id,如下:


Best chemical ID : 446 Best chemical ID max. deviation, % : 14.01



Summary of all IDs with max. DOD deviation below 15%

Chem ID max DOD error, % Max R deviation, ratio
0 0 0

Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge.

max. deviation是14%,电池是4串的磷酸铁锂电池,请问这个ID可以用吗?