This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求推荐便宜的单路宽输入DCDC转换器和4路输出DCDC转换器

Other Parts Discussed in Thread: LM25010, TPS54140, TL2575-ADJ, TPS65400, LMR14020

要求:便宜

1)、输入范围达到5~40V,单路输出应用5V,电流1A就够;

2)、输入5V左右,输出4路满足:3.3V@0.5A、1.2V@1A、1.8V@1A、2.3V@2.5A;

一定要便宜,求推荐。

  • Hi

        TL2575-ADJ,  TPS54140,LM25010 都相对偏低,但是注意这些芯片都不能实现100%duty,所以最低输入电压不能是5V, 你需要提升一些输入电压。

       TL2575-ADJ:http://www.ti.com.cn/product/cn/TL2575-ADJ/description

       单个芯片实现4个DC/DC降压,同时满足电流需求(不建议用LDO,功耗太大)这样的芯片应该是没有的,能否用2个芯片来做?

  • 可以啊,用两个,有什么推荐吗?

    也就是输入5V,输出3.3/1.2/1.8/2.3V其中的两个;

  • Hi

        还真找到一个4路DC/DC的, TPS65400:   http://www.ti.com.cn/cn/lit/ds/symlink/tps65400.pdf   价格也不贵。(相比2片DC/DC应该是便宜的)

  • 1)LMR14020
    2)TPS65400