Other Parts Discussed in Thread: LM25010, TPS54140, TL2575-ADJ, TPS65400, LMR14020
要求:便宜
1)、输入范围达到5~40V,单路输出应用5V,电流1A就够;
2)、输入5V左右,输出4路满足:3.3V@0.5A、1.2V@1A、1.8V@1A、2.3V@2.5A;
一定要便宜,求推荐。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM25010, TPS54140, TL2575-ADJ, TPS65400, LMR14020
要求:便宜
1)、输入范围达到5~40V,单路输出应用5V,电流1A就够;
2)、输入5V左右,输出4路满足:3.3V@0.5A、1.2V@1A、1.8V@1A、2.3V@2.5A;
一定要便宜,求推荐。
Hi
TL2575-ADJ, TPS54140,LM25010 都相对偏低,但是注意这些芯片都不能实现100%duty,所以最低输入电压不能是5V, 你需要提升一些输入电压。
TL2575-ADJ:http://www.ti.com.cn/product/cn/TL2575-ADJ/description
单个芯片实现4个DC/DC降压,同时满足电流需求(不建议用LDO,功耗太大)这样的芯片应该是没有的,能否用2个芯片来做?
可以啊,用两个,有什么推荐吗?
也就是输入5V,输出3.3/1.2/1.8/2.3V其中的两个;
Hi
还真找到一个4路DC/DC的, TPS65400: http://www.ti.com.cn/cn/lit/ds/symlink/tps65400.pdf 价格也不贵。(相比2片DC/DC应该是便宜的)