This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5160芯片带载输出电压跌落——问题进展

Other Parts Discussed in Thread: LM5160

 各位好!经过这几天的定位,隔离输出带载的基本原因是找到了,应该是因为变压器初级和次级的匝数过多(向变压器厂家咨询了,初级将近70匝,次级对初级匝数比为3.125)导致线圈阻值太大,阻值会分压,所以输出电压跌落。我实测了次级的阻值,将近3.5欧姆,确实比较大。而且给非隔离输出Vpri带载,在整个输入电压范围内,Vpri还是比较稳的。就像TI的工程师的分析的,应该是变压器的问题。
现在我让厂家重新绕了变压器,磁芯是EF20,初级感量有50UH和80UH,漏感2UH左右。初级匝数是十几匝(具体是多少匝得问问变压器厂家了,这个厂家只会按照我们的要求绕变压器,也没有什么经验),次级对初级匝数比为3.125左右,这次匝数少了所以线圈阻值比较小了,我实测了新的变压器的线圈阻值,初级0.09欧姆,每个次级是0.3欧姆,阻值是比较小了。但是发现另外一个问题,不管50UH还是80UH的变压器,基本上在整个输入电压范围20VDC到56VDC(尤其高压输入的时候),带载5W,初级电流都超过了2.1A。只是20VDC输入到40VDC输入的时候,输出电压看不出有什么跌落,还是基本可以保持。但是44VDC以上的时候,运行一分钟左右,输出电压就跌落了,台阶式的跌落,跌落的时候变压器初级电路明显增大,三四安培都有。我觉得应该是变压器饱和了。附件有44VDC输入,带载5W,刚开始输出电压还有的时候的变压器初级电流波形,各位看看。
我们公司是上市公司,但是比较难找到有效高效的技术支持。这个项目比较重要,眼下比较急,我今天也加班过来调试,但是这个电源还是有问题,应该问题还是在变压器上面。各位是否可以帮忙给个合理的变压器参数,包括初级感量、初级匝数、匝比、线圈阻值、绕法等(目前的变压器绕法就是先初级后次级线圈,没有其他的了),不胜感激。这个电源的需求是:输入电压范围20VDC到56VDC,隔离输出两路,每一路都是24V输出,总功率5W(瞬态可以达到10W)。我的QQ 491099858,论坛沟通感觉效率比低,项目比较急,方便的话加我的QQ沟通,麻烦各位了!!!当前的原理图.pdf

LM5160带载输出电压跌落.pdf各位好!我在使用LM5160芯片时候遇到一个问题。我设计的电源输入电压范围20-55VDC,隔离输出两路24V,总功率10W。在24VDC输入的时候,空载输出电压28V左右。但是给其中一路带载0.1A,该路电压跌落到13.2V,但是非隔离输出的电压Vpri在带载和不带载的时候都比较稳,是9V。我使用的变压器初级感量50UH,每一路次级对初级的匝数比为3.1左右。带载时候变压器初级峰值电流为0.6A左右,变压器也应该没有饱和。请问为什么带载的时候输出电压会跌落?如何解决?谢谢。

  • Hi
    隔离输出异常时是否影响到非隔离9V? 应该只可能是变压器的问题。
  • 带载的时候,非隔离的9v基本是比较稳的,只有零点几伏特的变化。我也感觉是变压器有问题。我用的是ef20的磁芯,次级匝数比初级是3.125左右,初级感量50uh,变压器也没有饱和,请问变压器参数有问题吗?是否可以帮忙给个变压器参数。

  • Hi
    变压器是你绕的,还是买的成品?如果是自己买的,有没有测试过其规格是否符合?感量,漏感,电流之类。
  • 你好,估计变压器耦合太差。抓个电压电流波形看看,谢谢。
  • 你好!我更新了帖子。之前的输出电压跌落是因为变压器线圈阻值太大。使用新的变压器有发现问题了,变压器初级电流很大,变压器应该是饱和了,所以输出电压跌落。这个项目比较重要,眼下比较急,我今天也加班过来调试,但是这个电源还是有问题,应该问题还是在变压器上面。是否可以帮忙给个合理的变压器参数,包括初级感量、初级匝数、匝比、线圈阻值、绕法等(目前的变压器绕法就是先初级后次级线圈,没有其他的了),不胜感激。这个电源的需求是:输入电压范围20VDC到56VDC,隔离输出两路,每一路都是24V输出,总功率5W(瞬态可以达到10W)。我的QQ 491099858,论坛沟通感觉效率比低,项目比较急,方便的话加我的QQ沟通,谢谢了!!!
  • 你好!我更新了帖子。之前的输出电压跌落是因为变压器线圈阻值太大。使用新的变压器有发现问题了,变压器初级电流很大,变压器应该是饱和了,所以输出电压跌落。这个项目比较重要,眼下比较急,我今天也加班过来调试,但是这个电源还是有问题,应该问题还是在变压器上面。是否可以帮忙给个合理的变压器参数,包括初级感量、初级匝数、匝比、线圈阻值、绕法等(目前的变压器绕法就是先初级后次级线圈,没有其他的了),不胜感激。这个电源的需求是:输入电压范围20VDC到56VDC,隔离输出两路,每一路都是24V输出,总功率5W(瞬态可以达到10W)。