This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lm5118 空载时频率会发生变化



设计指标:输入电压7~28V,输出电压15V,输出电流1A

问题:轻载时,当输入电压大于20V时,输出电压虽然稳定,但系统频率会发生变化,请问这个是正常的吗?还是因为什么原因造成的?可以通过调节哪些参数可以更正?

其中Q301是上管,Q302是下管