This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

?TPS40210,完全按照PMP8621原理图设计的PCB,有些能输出300V,另外一些没有输出

Other Parts Discussed in Thread: TPS40210, PMP8621

?TPS40210,完全按照PMP8621原理图设计的PCB,有些能输出300VDC,另外一些输出21VDC

1、完全按照PMP8621文档进行TPS40210设计,输入24VDC,要求输出300V。

2、电路做出来后,发现,有一些能输出300V,另外一些输出21VDC。

3、输出21VDC的,查了下,用示波器和万用表测量了下PIN2引脚(SS),此时为0V;

    在此种情况下,如果把Q1 Si2328DS去掉,PIN2(SS)引脚电平恢复到7.3V(正常时候应该是7.3V);

PS:在试验过程中,可以保证所有芯片、其他原材料质量和焊接焊接质量;

请TI工程师帮忙分析。

感谢了

http://www.ti.com.cn/tool/cn/pmp8621#technicaldocuments