This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5150上电时瞬间输入电流过大



Dears

1、使用LM5150时,Vin=6V,Vout=7.5V,当上电时,LM5150输入端会有短暂电压跌落,测试发现当Boost启动时会有个较大的尖峰电流,应该是这个大的尖峰电流导致Vin出现的跌落,从而导致我的系统重启(是不允许的),各波形见下图:3通道(蓝色)为Vin,  2通道(红色)为Vout ,1通道(黄色)为输入电流 Iin ,

问题:(1)LM5150启机时,会有较大的尖峰电流是否正常?

           (2)是否有方法可以限制这个上电Iin峰值电流,如同构CS脚的电阻?CS脚电阻和限流值的对应关系是怎样的,DEMO原理图中额定2A负载对应的是7m欧,建议的供电电源限流值20A(为什么要这么大?)

            (3)我的目的是要6V上电能正常启机,不会重启,可有什么建议