This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54318出现低压导致开机上电1/10几率黑屏



分析过程:

实测电压:1.20V

实测电压:1.27V

根据DDR规格书要求,U11供电电压不低于1.283V

根据I.MX6规格书要求,U4供地电压低于1.35V会造成处理器降频

需要帮忙分析:

根据实测电压1.27V(U4标准值为1.4V),1.2V(U11标准值为1.35V)推算U4参考电压VF=0.7324V,U11参考电压VF=0.7062,

与其规格书描述的0.8V 1%不符,

怀疑CPU 1.4V,DDR1.35V位置电压过低是CPU重启和上电无法启动的原因。

两位置电压过低均会有CPU重启,无法启动,运行异常的风险,请问有什么原因会导致这种情况?