在使用TPS54628做一个无线充的电源,现在PP遇到一个问题:
负载有时候无法在短时间(<2S)识别到电源:
在16V的适配器供电的情况下,同一个负载在进行多次充电的情况下,有10%的机会会出现以上现象。其实都在<1S的时候会识别充电。
如果改用12的电池供电情况,则不会出现这不良现象。
目前客户是按照5V/6A去设置参数,在无线充不带负载情况下,功耗为20mA的输出。
想知道在适配器及电池供电的情况是什么引起这么大区别。在TPS54628怎么去调整。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在使用TPS54628做一个无线充的电源,现在PP遇到一个问题:
负载有时候无法在短时间(<2S)识别到电源:
在16V的适配器供电的情况下,同一个负载在进行多次充电的情况下,有10%的机会会出现以上现象。其实都在<1S的时候会识别充电。
如果改用12的电池供电情况,则不会出现这不良现象。
目前客户是按照5V/6A去设置参数,在无线充不带负载情况下,功耗为20mA的输出。
想知道在适配器及电池供电的情况是什么引起这么大区别。在TPS54628怎么去调整。
即可地方需要修改一下,输出端电解改为陶瓷电容,容值上100uF足够了。
可以尝试移除输入端的滤波电感看是否还有延时,10uH电感太大了,上电瞬间需要预充电的时间过长,