目前我使用bq24259芯片设计的电路中,想要实现适配器供电与电池供电的选择,电池没电时用适配器充电。芯片没有主机控制(应该可以吧。。。),按默认设置工作。现在OTG,QON,PG,STAT,都没有连接(悬空),cs直接接电阻拉低,其他按推荐电路。当适配器接5v,2A适配器时,sys只输出约1.7V电压(应该3.5v左右),BAT引脚电压只有50mV左右(应该是3V多才对吧),请问大神们我的问题在哪里呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前我使用bq24259芯片设计的电路中,想要实现适配器供电与电池供电的选择,电池没电时用适配器充电。芯片没有主机控制(应该可以吧。。。),按默认设置工作。现在OTG,QON,PG,STAT,都没有连接(悬空),cs直接接电阻拉低,其他按推荐电路。当适配器接5v,2A适配器时,sys只输出约1.7V电压(应该3.5v左右),BAT引脚电压只有50mV左右(应该是3V多才对吧),请问大神们我的问题在哪里呢?
你好,
ILIM 引脚电阻选择10k,输入电流被限制在 IINMAX = (1V/RILIM) × KILIM =435(typ)/10000=0.0435A。可以换成较小的电阻,如数据手册上典型应用推荐的317欧姆 (1.5A max)。