Other Parts Discussed in Thread: UCC21521, UCC21520
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,您的问题应该是VDD与VSS之间的电压差小于芯片正常工作所需电压,导致该芯片进入了欠压保护状态。
以下是UCC21521的数据手册里的推荐参数,您使用的是UCC21521CDW,所以,如果您的VSS要设置为5V,那么VDD至少要20V以上才能够正常工作。所以您如果想要实现5V-12V的输出,您必须选择Driver output bias supply较小的芯片。如果还要选择UCC21521,应该选择UCC21521ADW,5V UVLO version这款。
后面是我的一个仿真,由于UCC21520有现成的TINA参考设计,二者的主要差别在于UCC21520是DIS PIN。所以我拿这款芯片来进行了仿真验证。
当VDD2=12V,VSS2=5V:OUTB没有输出
我们增加VDD的电压值,当VDD=13.8>5+8.7=13.7,VSS=5V:OUTB输出正常。
为了保险起见,建议VDD-VSS更大一些,留出一些余量。
如果还是有问题,建议您把您实际的原理图贴出来,标清楚各个节点的电压值。
您好,刚才图片都没有显示出来,请参照我的这个文档UCC21520.docx