This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65217C的PB_IN脚问题



这个引脚手册上说是内部上拉5V,可外接开关拉到地,低电平有效。

我在实际使用时,有些板子这个脚是悬空的,可以正常启动。但有些板子必须把这个脚拉一下低才能启动。

请问这个引脚 具体正确的接法应该是如何的。空间有限不用开关,就接上拉或者下拉电阻固定接行吗?

  • 看手册说是pb_in是接电池的时候,需要接一个开关,然后低电平触发开机

    我也是悬空的

    目前pmic上电电压都正常,不过时序没有测

    还有一个问题,我的板子全都起不来,uart0 保持3.3V高电平,tx,rx都是

    确认复位和sysboot都对

    不知你那边有啥建议没有?

  • Figure 24 (Global State Diagram) shows the possible power on scenarios. From the OFF state, USB or AC detection can cause a power on, so if they are used then PB_IN can be floating. If a start-up condition is needed without USB or AC being plugged in, then a falling edge on PB_IN needs to be generated.

    As noted in the upper right corner of Figure 24, if PB_IN is tied to GND, then after 8 s the device will reset (long key press, similar to a phone / smart watch / etc).
  • 你好,我想请问一下
    当前我的板子tps65217C 上电电压是4.5V
    复位信号保持3.3
    sysboot 配置正确
    现在在uart0上没有CCCC打印
    并且uart0 和tx 和 rx 都是3.3V
    我该怎么检查