Other Parts Discussed in Thread: BQ25606
我现在在做一个充电电路板,面积21*25mm,充电电流设定为800mA。
现在用它给3.5V的锂电池充电, 充电电流实测 810mA,芯片表面温度超过了65度,而且PCB表面也很烫。
想问一下有没有更好的方法提升散热效果。
我用的0.8mm的PCB,cu厚65微米。
或者有其他更合适的芯片适合我的应用。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.