This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
原理图如附件所示,用的是LM5119芯片,之前一直有在生产,大概有生产了5K套左右,现在发现一个问题,在大动态负载的情况下,会突然没输出,造成负载会重启。经检查发现,驱动波形不正常(如附件图片所示,只要是有这个转折的,一定会有问题),修理的方法是更换Cramp电容(应该是斜坡发生器的电容),目前用的是2.2NF,但是换了很多电容才能修好一台机器,试过换大或是换小,驱动波都不正常。请TI工程师帮我分析一下,这是什么问题,问题的根本原因是不是这两个电容,如果是这两个电容,需要用什么规格的电容才能解决这个问题?
Hi Johnsin,
您好,我今天拿出TI的DEMO板来测试(两年前从代理处获得),发现这两个电容对驱动波也一样存在这种影响,从一盘三星的2.2NF 10%的X7R电容中不断的换这两个电容,会有很漂亮的波形,但是很多情况也有差的波形,就是在上升的时候,在中间会有一个折弯的位置(如我前面上传的图差不多)。这两个电容在用法上有什么要求?要用什么材质的电容?是不是要确保这两个电容的容量非常接近? 偿试过改频率没有效果,改电感也没有效果,改MOS管也没有效果。我有四款PCB都是用同样的电路,都同样存在这个问题。另外,这四款板,都可以带电子负载12V @35A长时间工作没有问题,但是对于动态的负载就会出问题(输出会瞬间跌到比较低的电压,然后又恢复正常,这样会导致负载重启)。目前没有好的对策,所以请帮忙分析下是什么原因导致。万分感谢·!