This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25504仿真 VBAT_OK与VSTOR输出电压问题



模拟在没有外部太阳能电池输入、VBAT接3V电池情况下,想下确认VSTOR的输出电压。

系统设置如下:

1、UV、OV、VBAT_OK设置同EVK设置即OV:3.1V,UV:2.2V;

2、VBAT_OK高电平:2.8V,VBAT_OK低电平:2.4V;

3、负载用10K电阻来表示;

4、在VSTOR和VBAT_OK之间连接了一个NcH+Pch的MOSFET(EM6M2)。

实际模拟发现当电池电压(VBAT)低至1.3V的时候,VBAT_OK才置低,这个原因不太理解,望高手们指点一下。

附件:仿真原理图和EM6M2手册。