This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

恶劣供电环境的DCDC选型

Other Parts Discussed in Thread: LMR33620, LMR14050, LMR14030

您好,

目前项目中在选用一颗DCDC, 使用场景如下。

DC Input:   7.5V~30V, 供电为锂电池供电,且锂电池也同时为瞬间负载变化特别大的无刷电机供电,所导致的情况。DC输入端,瞬间电压波动特别大,大概在~上下10V/100ms的电压波动

DC Output: 5V   输出电压波动小于100mV

I_OUT: 2A          输出端负载相对稳定

请问:

该使用场景下,推荐什么拓扑结构的电源,或者请帮忙推荐DCDC型号。 十分感谢