您好,
目前项目中在选用一颗DCDC, 使用场景如下。
DC Input: 7.5V~30V, 供电为锂电池供电,且锂电池也同时为瞬间负载变化特别大的无刷电机供电,所导致的情况。DC输入端,瞬间电压波动特别大,大概在~上下10V/100ms的电压波动
DC Output: 5V 输出电压波动小于100mV
I_OUT: 2A 输出端负载相对稳定
请问:
该使用场景下,推荐什么拓扑结构的电源,或者请帮忙推荐DCDC型号。 十分感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
很多DCDC都可以实现。关键看抗干扰
LMR14030,频率可以到2.3MHz, 电流3.5A,输入电压波动条件下也可以使用,因为这个是可以用于汽车电池的第一级使用(Start-stop时,电池电压波动范围7-36V),所以可以承受输入的电压波动