使用一个BQ25703充电IC,但是在调试时发现CHRG_OK管脚一直为低,插入DC电源后只有零点几伏电压,一直为低,CHRG_OK直连到CPU管脚,配置为上拉。DC输入为12V,VBUS为12V,查看0x20寄存器也没有报fault,想请问下这个是什么原因导致的呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
测得其他电压如下,
VBUS 12V
ACN/ACP 12V
REGN 6V
CHRG_OK 0.28V
VDDA 6V
HIDRV1 6.8V~7.4V
LODRV1 2.8V~3.1V
SW1 4.6V~5.0V
BTST1 10.5V~10.9V
BTST2 10.5V~10.9V
SW2 4.6V~5.0V
HIDRV2 7.6V~8.1V
LODRV2 2.0V~2.2V
VSYS 8.7V
BATDRV 0.47V
SRP 8.7V
SRN 8.7V
CELL_BATPRES 2.47V
IADPT 0V
IBAT 0V
PSYS 0V
COMP1 1.25V
COMP2 1.13V
PROCHOT 0.05V
ENZ_OTG 0V
想请问下什么情况会导致CHRG_OK一直为低呢?