This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703 CHRG_OK脚一直为低



使用一个BQ25703充电IC,但是在调试时发现CHRG_OK管脚一直为低,插入DC电源后只有零点几伏电压,一直为低,CHRG_OK直连到CPU管脚,配置为上拉。DC输入为12V,VBUS为12V,查看0x20寄存器也没有报fault,想请问下这个是什么原因导致的呢?

  • 量一下其它管脚是否有输出电压。
  • 测得其他电压如下,

    VBUS                        12V

    ACN/ACP                  12V

    REGN                        6V

    CHRG_OK               0.28V

    VDDA                        6V

    HIDRV1                   6.8V~7.4V

    LODRV1                    2.8V~3.1V

    SW1                         4.6V~5.0V

    BTST1                     10.5V~10.9V

    BTST2                      10.5V~10.9V

    SW2                         4.6V~5.0V

    HIDRV2                 7.6V~8.1V

    LODRV2                    2.0V~2.2V

    VSYS                       8.7V

    BATDRV                    0.47V

    SRP                            8.7V

    SRN                            8.7V

    CELL_BATPRES       2.47V

    IADPT                         0V

    IBAT                            0V

    PSYS                           0V

    COMP1                        1.25V

    COMP2                          1.13V

    PROCHOT                   0.05V

    ENZ_OTG                       0V

    想请问下什么情况会导致CHRG_OK一直为低呢?