This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23751PWP 4 类 PoE 反激转换器 (12V@2.125A) 参考设计,在测试的时候没有12V输出



设计参考资料:www.ti.com.cn/.../PMP11254

在测试的时候整流桥电压有提高到51V,但是没有保持在51V。D12有6~7.1V的电压到芯片电源,R41电阻没有250K的信号输出,GATE引脚输出信号不稳定导致MOS管直接烧了。请教一下我该如何去排查这个故障,有没有大神知道的。