This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
专家,您好!关于MC33063调试过程中发现的问题,特向专家请教一下,谢谢!
问题:MC33063电路上的电感有很大的啸叫声,测试发现MC33063的PIN1&PIN8输出波形有点奇怪,Ton和Toff的时间为啥是变化的?按照datasheet(如下图)里讲到的在选定Ct电容后,Ton和Toff的时间应该是固定的,芯片的开关频率也应该是固定的,请问是什么原因导致芯片工作的频率是变化的?这个问题会导致电感发生啸叫声吗?
MC33063电路设计及相关测试波形如下:
示波器测到MC33063的PIN3输出波形
示波器测到MC33063的PIN1(CH1)&PIN8(CH2)输出波形
Hi
请确认一下如下问题:
1. 5V输入是否很稳定? 较小负载,空载(或者<10mA)测试时,电感是否也啸叫?(按照你的测试最大负载电流时100mA)
2. PBO3316-221是220uF 0.8A电感,请测试一下电感的实际饱和电流。
这个电感无论电流还是电感值都是可以满足设计要求的。叫是因为电路工作在不稳定状态吧,从图中也可以看到这一点。