使用TPS5460,输入电压24V,输出12V ,4A,电路如下:
现在输出带3欧,100W水泥电阻,测量发现,输出端电压从11.95V到5V左右不停地跳变,请给予支持。
1.用示波器测量SW管脚,在电感33uH的时候,波形如下:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用TPS5460,输入电压24V,输出12V ,4A,电路如下:
现在输出带3欧,100W水泥电阻,测量发现,输出端电压从11.95V到5V左右不停地跳变,请给予支持。
1.用示波器测量SW管脚,在电感33uH的时候,波形如下:

电容参考的事SLVy863里面24V 转5V的 TPS54560EVM-515 Schematic电路做的。
EVM手册里面的C5是4700pF,等效4.7nF,不是4.7uF