Other Parts Discussed in Thread: TPS51100
以上是我用TPS51100为DDR2做的稳压电路,输出DDR2的参考电压0.9V。问题是去掉这部分电路,整个电路板的输入功率是1W左右,焊上这部分电路,输入功率大约是7W左右,电流猛然增大,是不是我哪里接的不对呢?输入电压是12V,中间有各种稳压芯片变成TPS51100所需的5V和1.8V。而5V和1.8V的电压电流基本是正确的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS51100
以上是我用TPS51100为DDR2做的稳压电路,输出DDR2的参考电压0.9V。问题是去掉这部分电路,整个电路板的输入功率是1W左右,焊上这部分电路,输入功率大约是7W左右,电流猛然增大,是不是我哪里接的不对呢?输入电压是12V,中间有各种稳压芯片变成TPS51100所需的5V和1.8V。而5V和1.8V的电压电流基本是正确的
Hi
建议直接断开12V到5V之间的电源电路,直接通过外接5V/1.8V电压给到TPS51100的输入(注意电压反灌,断开与12V那边的连线),然后测试5V的实际功耗,正常而言正常空载电流1.2mA.(VS3 = VS5 = 5 V)
说先需要确认的是1w的功耗是否耗在TPS51100, 按照你之前的测试没有带DRR2有1W的功耗,代表没有短路,短路后电流应该比较大,功耗应该不止1W.
在带上DRR2后,功率增加6W,说明TPS51100输入的电流应小于3A(3A*1.8V=5.4W, 修正), 从这个上面看TPS51100是可以正常转换电压的,芯片应该没有问题。而剩下的超过0.6W, 则很可能是因为上一级的转换导致的。