我用tps51116芯片给DDR3供电,s3 s5直接用100K的电阻上拉,输出1.5V正常,但是S3 S5引脚用外部PGRGOOD信号控制,上拉电阻测量只有1K多,测量芯片的输出电压只有0.5V左右,这种情况会是什么问题导致的呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用tps51116芯片给DDR3供电,s3 s5直接用100K的电阻上拉,输出1.5V正常,但是S3 S5引脚用外部PGRGOOD信号控制,上拉电阻测量只有1K多,测量芯片的输出电压只有0.5V左右,这种情况会是什么问题导致的呢?
能否说明下接R442及C515的作用??
建议对照下TI的参考设计:
http://www.ti.com/tool/tps51116evm-001
http://www.ti.com/lit/ug/sluu202a/sluu202a.pdf
额 我太着急了 写错了 不是R442 是焊接R462就变成0.5V了
R442没焊接,所以R442 C515是没什么用的