This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

pl455采集电压



遇到的问题是pl455采集电压时都是0,但是通讯是正常的,指令响应也是正常的,只是返回的电压数据位都是0;

不清楚是什么问题导致:硬件?软件?

问题详细描述在附件中。

2402.pl455问题描述.docx

  • 下面链接是bq76PL455A-Q1 Software Design Reference您参考一下
    www.ti.com.cn/.../slva617a.pdf
  • 我们已经验证过了,可以通过发送指令读取电压和调整选取通道的数量。在调试过pl455之后我们进行了1428和1499均衡的调试。等回过头来想根据电压进行均衡时发现采集出来的电压为0V,您给的手册我们已经确认好用,而且指令能够响应,现在的问题是:读取得到的电压为0V有几种可能。通过进一步测试,我们发现电荷泵的-5V那端实际电压只有-1V左右。我们尝试用其他办法确认软件or硬件问题,读取了模拟和数字的温度,发现数字温度正常,换算后有32度。 而模拟温度也是0,因此我们通过结构框图推测,MUX没有工作,也就是没有做选通(等待TI工作人员确认),能否提供MUX是否工作的确认方法,输入是什么,输出应该是什么。从现在的现象看,pl455能够正常响应指令,比如选择2个电池采样和选择1个电池采样,示波器的信号位数是不一样的。所以pl455不是完全烧毁的那种坏掉,只是部分功能缺失,我们也怀疑这可能是某种锁死或者保护在起作用,请TI工作人员提供可能导致类似现象的可能,以及解决方案。 我们诚挚的希望解决这样的问题,如果有必要,我们可以把EVM1402开发板邮寄过去,请你们来帮忙解决。非常感谢您的回复,期待针对上述问题得到您的指导。