我用的LM3478做的反激。DC-DC,VIn:9~18v Vour:12V Iout:1.7A.发现问题
1、输入上电时容易时容易上电输入电压拉低,输入电压12V拉低为4V多,开关管占空比100%,只 有供电正常,接上才行,无论空载或带载。是什么造成的?
2、我占空比按照45%设计,是否这种情况需要占空比设定的大一点才好呢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
MOS管没有烧。是的占空比100%了,后边是空载就这样。应该是一上电电压就被拉低到4V左右,占空比就100%,引脚波形如附件所示8712.新建 Microsoft Word 文档.docx
请教一下各位这个,图是什么意思,是占空比越大,Vsen阈值电压低的意思吗?新建 Microsoft Word 文档 (2).docx
换一个输入电源是怎么换的?如果是12V的电源,不能输出12V,你应该先检查前端电源的问题,需要看一下这个电源工作在什么状态?是否是过流保护了?然后再分析后面电源的情况。
有没有实验室用的直流电源?用这个看看。