Other Parts Discussed in Thread: LM340
各位专家,你好:因为要提供5V/1A给液晶屏背光供电,所以我选用线性三端稳压器LM340-5.0V,接法以下如图三端输入端连接开关电源12V、输出端接了液晶屏,现象是LM340非常烫,输出电压瞬间跌落为2V左右,请问是什么原因如何解决呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
感谢各位专家回复,首先直接用5V开关电源给液晶屏供电实测电流850mA左右,然后我在图上电路中在输出端和电源地上并联了不同阻值纯电阻5欧姆和10欧姆(模拟负载情况),结果还是三端很烫,输出电压瞬间跌落到2V左右很不正常,随后我也考虑热保护问题,我买的封装是TO-263,加过散热器,但是实验结果还是一样。我使用的参数都符合LM340数据手册上的要求,请问还有什么情况会造成我这种情况呢?
另外线性三端稳压器和开关型三端稳压器优缺点我也有所了解,我如用线性类三端尤其封装用的是TO-263或SOT-223和压差较大情况下(类似Vin=12V,VOUT=5V)要特别注意什么呢?若有注意的情况数据手册那里有些这方面注意情况?还有我使用的参数符合我选择LM340规格要求吗?