您好!我得到几片LM5007,但是丝印第一行是MDAG,第二行是S81B,我从TI官网下载了LM5007的datasheet,按照典型电路搭了一个电路,元件参数都对,但是电路工作不正常,输入20V一下工作还可以,输入高了,输出纹波相当大,而且输入达到60V芯片就烧坏了,datasheet里不是说75V吗?我得到的芯片是不是假的???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!我得到几片LM5007,但是丝印第一行是MDAG,第二行是S81B,我从TI官网下载了LM5007的datasheet,按照典型电路搭了一个电路,元件参数都对,但是电路工作不正常,输入20V一下工作还可以,输入高了,输出纹波相当大,而且输入达到60V芯片就烧坏了,datasheet里不是说75V吗?我得到的芯片是不是假的???
首先,你买的产品的full P/N是什么?
下面我列了一个LM5007SD/NOPB 的丝印format:
Topside Symbol : NS-NGT8 01
+--------------------+
! ! \NS/ = NATIONAL LOGO
! \NS/ ! YM = YEAR MONTH DATE CODE
! YMLLLLP ! LLLL = ASSY LOT CODE
! L00031B ! P = PRIMARY ASSY SITE CODE
! ! (PER QSS 005-120)
! O !
+--------------------+ 2 CHARACTERS MAX LINE 1
O - PIN 1(MARKED DOT) 7 CHARACTERS MAX LINE 2
7 CHARACTERS MAX LINE 3
这颗料的丝印format:
Topside Symbol : NS-DGK8 01
+--------------------+
! !
! YMLL ! YM = YEAR MONTH DATE CODE
! S81B ! LL = LAST 2 DIGITS IN
! ! ASSY LOT CODE
! O !
+--------------------+
O - PIN 1(NOTCH ON PKG) 4 CHARACTERS MAX LINE 1
4 CHARACTERS MAX LINE 2
Hi
问题应该出在你的输入电容上?
请确认你的输入电容耐压是否真的是100V, 建议您采用4.7~10uF的电容,耐压100V(以及以上)的低ESR电容, Layout上尽量靠近芯片Vin脚。(上述目的是为判定输入电容的问题,后续实际上您可以采用1~10uF电容, 建议多个并联以降低ESR)
输出纹波比较大,同样建议你选择低ESR的陶瓷电容,并且容量要够。(datasheet第三页电路选的是15uF的钽电容,注意要选择质量较好的低ESR钽电容,或者您改为22uF陶瓷电容也可以,另外R6是不需要的,这里应该是标示为输出电容的ESR)
Hi
经查询,S81B是LM5007的marking , 或者你可以在TI官方网站上申请样片。
另外从你的测试看,20V时测试还行,代表芯片功能上没有问题,如果是伪劣芯片,功能上肯定不对,而芯片表面上的marking很容易伪造,不能说明问题。所以建议你按之前的回复确认。