This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5007求鉴定

Other Parts Discussed in Thread: LM5007

您好!我得到几片LM5007,但是丝印第一行是MDAG,第二行是S81B,我从TI官网下载了LM5007的datasheet,按照典型电路搭了一个电路,元件参数都对,但是电路工作不正常,输入20V一下工作还可以,输入高了,输出纹波相当大,而且输入达到60V芯片就烧坏了,datasheet里不是说75V吗?我得到的芯片是不是假的???

  • 首先,你买的产品的full P/N是什么?

    下面我列了一个LM5007SD/NOPB 的丝印format:


       Topside Symbol         : NS-NGT8                                             01   
         +--------------------+                                                          
         !                    !         \NS/ = NATIONAL LOGO                             
         ! \NS/               !           YM = YEAR MONTH DATE CODE                      
         ! YMLLLLP            !         LLLL = ASSY LOT CODE                             
         ! L00031B            !            P = PRIMARY ASSY SITE CODE                    
         !                    !                 (PER QSS 005-120)                        
         ! O                  !                                                          
         +--------------------+          2 CHARACTERS MAX LINE 1                         
          O - PIN 1(MARKED DOT)          7 CHARACTERS MAX LINE 2                         
                                         7 CHARACTERS MAX LINE 3                        

  • LM5007MM/MSOP-8,我得到的丝印仅仅是第一行MDAG,第二行S81B,其它什么都没有!

  • 这颗料的丝印format:

    Topside Symbol         : NS-DGK8                                             01    
         +--------------------+                                                           
         !                    !                                                           
         ! YMLL               !           YM = YEAR MONTH DATE CODE                       
         ! S81B               !           LL = LAST 2 DIGITS IN                           
         !                    !                ASSY LOT CODE                              
         ! O                  !                                                           
         +--------------------+                                                           
          O - PIN 1(NOTCH ON PKG)        4 CHARACTERS MAX LINE 1                          
                                         4 CHARACTERS MAX LINE 2                          

  • YMLL是用数字还是字母?

  • 没看PDF文档,输入即使允许75V也应该是正常工作情况下,你输出纹波很大是不是出于震荡状态?如果是,那再60V损坏不一定是假的器件,因此首先应该查找纹波大的原因。

  • Hi 

       问题应该出在你的输入电容上?

       请确认你的输入电容耐压是否真的是100V, 建议您采用4.7~10uF的电容,耐压100V(以及以上)的低ESR电容, Layout上尽量靠近芯片Vin脚。(上述目的是为判定输入电容的问题,后续实际上您可以采用1~10uF电容, 建议多个并联以降低ESR)

       输出纹波比较大,同样建议你选择低ESR的陶瓷电容,并且容量要够。(datasheet第三页电路选的是15uF的钽电容,注意要选择质量较好的低ESR钽电容,或者您改为22uF陶瓷电容也可以,另外R6是不需要的,这里应该是标示为输出电容的ESR) 

  • Hi

        经查询,S81B是LM5007的marking , 或者你可以在TI官方网站上申请样片。

        另外从你的测试看,20V时测试还行,代表芯片功能上没有问题,如果是伪劣芯片,功能上肯定不对,而芯片表面上的marking很容易伪造,不能说明问题。所以建议你按之前的回复确认。