Other Parts Discussed in Thread: TPS5450
大家好,帮我看下是什么问题,第一次使用TPS5450,输入DC24V 输出-15V0.6A,我是上电就把IC烧坏了,都冒烟了,不知道哪里来的这么大的电流,把里面的MOS烧坏;这个现象几乎总是存在的,换了几次IC都是一样的现象。输出正电压目前调试都没有问题。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS5450
大家好,帮我看下是什么问题,第一次使用TPS5450,输入DC24V 输出-15V0.6A,我是上电就把IC烧坏了,都冒烟了,不知道哪里来的这么大的电流,把里面的MOS烧坏;这个现象几乎总是存在的,换了几次IC都是一样的现象。输出正电压目前调试都没有问题。
非常感谢Johnsin Tao:
1.后面我又将输入电压改到18-20V,测试结果就是没有一上电就烧掉,但是带负载上电多上电几次还是会烧IC,搞不懂?24V转-15V我这个板有3路,PCB有些差异,如图所示,但是结果都是一样的。
2.之前我们的电源板也有这路24V转-15V,今天我反复测试就是不坏,最高电压达到了41V左右,这个才是正常现象。后面又有个奇怪的详细,我拿了之前的电源板空板,只焊接了24V转-15V电路,测试结果也是烧坏IC。
3.我想问下,TPS5450如果散热合理,最大功率可以做到30W左右吧,
4.我的原理图没有问题吧,PCB应该不会有太大问题。24V转-15V0.6A 它的占空比是多大,贴片电感感量多大合理? 不知道改哪里了?
补充下,今天又试了下,空载10V正常,然后加载从0到0.5A,正常工作,空载到0.2A切换,芯片就烧坏了。