做一个手持设备,需要用到TPS63020,我是按照WEBENCH参考设计画的图纸,如下。其中PS/SYNC引脚已经默认接GND。但是在实际中测试时(只给MCU供电,MCU进入低功耗模式后)发现TPS63020在轻负载下(MCU已经低功耗,系统无其它设备)静态电流大概有7-8ma。这是什么问题引起的?PS/SYNC以及接GND。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
做一个手持设备,需要用到TPS63020,我是按照WEBENCH参考设计画的图纸,如下。其中PS/SYNC引脚已经默认接GND。但是在实际中测试时(只给MCU供电,MCU进入低功耗模式后)发现TPS63020在轻负载下(MCU已经低功耗,系统无其它设备)静态电流大概有7-8ma。这是什么问题引起的?PS/SYNC以及接GND。
Hi
按照你的条件,1.5A输出时效率应该在90%左右,77%是明显偏低的。
验证Powersaving下静态电流,你需要将输出的磁珠拿掉,让其Io=0mA, 如果此时消耗仍然在8mA左右,有可能是芯片存在问题,建议你换芯片看看(注意芯片来源需要是TI授权代理商或者免费样片,不能来自电子市场)
效率偏低不排除也是芯片问题造成的,但是要注意你选择的电感是饱和电流足够DCR尽量小的功率电感。
输出精度比较差,只要注意反馈电阻精度和layout。