This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1静置一段时间,电量会下降的问题

Other Parts Discussed in Thread: BQSTUDIO

现在我司生产了20块电池来专门进行问题测试,装配过程如下:

1.先对板子进行硬件测试,烧录gauge固件,然后烧录MCU固件,然后校准电压,温度;

2.装配电芯,焊接BMS板子,安装电池外壳;

3.对电池进行电流校准;

4.发送IT_ENABLE指令(该指令在电压基本稳定后才发送的),然后发送SEAL指令,所有电池进行完这一步,电量基本都在70%-73%;

5.对电池静置;

现象:现在已经静置了3天,不断记录数据,发现有16块电池电量明显下降,有10块下降超过15%,有3块下降超过20%,最低的一块下降到了44%,我将其中两块的gauge进行复位操作,电量又回到70%左右,所有电池开路电压基本没有变化。现在我很是头疼,还是我操作有问题。

我在此申明一下:化学ID绝对没有问题的