This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TPS61260失效问题

Other Parts Discussed in Thread: TPS61260

Dear All,

目前发现在130pcs中出现了7pcs的不良现象,现象描述如下:

1、当PCBA未烧录程序时,发现焊接该不良芯片的PCBA的电流超过3mA(正常的为2.5mA);

2、当PCBA烧录程序后,发现焊接该不良芯片的PCBA的电流为1.7mA(正常的为0.7mA);

3、输出电压2.4V情况下,芯片3号脚(FB)不良芯片的电压是1.045V,正常芯片的电压是0.512V,芯片规格书上写明电压是0.5V,不良芯片电压明显偏高;

根据以上问题,做了交叉验证,证明不良芯片确实是不良品,当换在另一块好的PCBA上也是不良;用好的芯片替换不良的芯片,该PCBA又变为良好,该芯片应用环境为在一款电容笔上,通过一节9号干电池供电,正常工作电流比较小;

该设计参考以下原理图:

芯片5号脚的波形:

Thanks!

测试130块,发现7块不良

  • Hi

        负载时mA级别的吗?

        测量此时输出电压是稳定的4.8V吗?   看起来是反馈脚有问题,7片不良都一个现象吗?   

  • Hi Johnsin,

    感谢您的回复;

    负载是mA级别的吗?

    >>是的,大约2mA左右;

    测量此时输出电压是稳定的4.8V吗?   看起来是反馈脚有问题,7片不良都一个现象吗?   

    >>通过一节9号干电池供电,输入电压为1.5V,经过TPS61260后输出应该为2.4V,7片不良都是一样的现象。

    Thanks!