This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610 使用磷酸铁锂电池 已经触发了COV 电量还是显示没充满 请问能否设置为 触发COV电量跟着更新为100%



 各位好!

        2S2P磷酸铁锂电池,

        满充电压设置为单节3.65V  

      Charge Term Taper Current   设置为 300mA

      Charge Term Voltage  设置为150mV

   充电器充电电压为7.30V  截止电流为100mA    

     当电池快接近充满的时候  SOC大约98%   其中一串电池电压升高至3.80V 触发COV过充保护  另外一节只有3.50V(咨询了电池厂家,磷酸铁锂特性就是如此  接近满电时电压变化比较大)   此时充电截止电流直接从700mA关闭   无法满足Charge Term Taper Current  持续40S检测 

请问各位专家,哪里可以设置  将Charge Term Taper Current 和 Charge Term Voltage  检测时间缩短    或者是触发COV更新SOC至100%吗